Part Number: TMS320F28069F-Q1
If possible, where to configure?
--
Thanks & Regards
Yale
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yale,
I'm copying the relevant sections from the TRM SPRUH18(starting at page 893); but the short answer is that yes it is possible:
15.3.2 Frame Synchronization Generation in the Sample Rate Generator
The sample rate generator can produce a frame-synchronization signal (FSG) for use by the receiver, the
transmitter, or both.
If you want the receiver to use FSG for frame synchronization, make sure FSRM = 1. (When FSRM = 0, receive
frame synchronization is supplied via the FSR pin.)
If you want the transmitter to use FSG for frame synchronization, you must set:
• FSXM = 1 in PCR: This indicates that transmit frame synchronization is supplied by the McBSP itself rather
than from the FSX pin.
• FSGM = 1 in SRGR2: This indicates that when FSXM = 1, transmit frame synchronization is supplied by the
sample rate generator. (When FSGM = 0 and FSXM = 1, the transmitter uses frame-synchronization pulses
generated every time data is transferred from DXR[1,2] to XSR[1,2].)
In either case, the sample rate generator must be enabled (GRST = 1) and the frame-synchronization logic in
the sample rate generator must be enabled (FRST = 0).
15.3.3.1 Operating the Transmitter Synchronously with the Receiver
When GSYNC = 1, the transmitter can operate synchronously with the receiver, provided that:
• FSX is programmed to be driven by FSG (FSGM = 1 in SRGR2 and FSXM = 1 in PCR). If the input FSR has
appropriate timing so that it can be sampled by the falling edge of CLKG, it can be used, instead, by setting
FSXM = 0 and connecting FSR to FSX externally.
• The sample rate generator clock drives the transmit and receive clocking (CLKRM = CLKXM = 1 in PCR).
Best,
Matthew