This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multi-core design

I have a quick question for TI.

Are there any plans on making a homogeneous multicore chip using the C2000?  I am envisioning a multicore F28335.

TI currently offers many heterogeneous multicore chips but does not appear to offer any homogeneous multicore. 

The main reason for a preference for a homogeneous multicore is that the developer(s) and maintainer(s) will only have to know one core architecture and still have the advantage of parallel computing in a single package.  Also, code reuse will be much easier.

If real estate is an issue, having a chip where one C2000 core has FPU support and the other doesn't is still useful.  Just don't sacrifice RAM space, please.

 Also, please make sure it'll be available in a non-BGA package.  Automotive and High Temp would be execellent.

 

Just a thought.  Best Regards.

-quark