This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: I need to create the Structure Array of 8192 size in Flash Section which should have read/write options

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Hi.

       I want to store the array of 64K word in Internal flash section, these data will be read 2 byte and write 2 byte and I want to use Sector 8 and Sector 9 ,If you have any reference code or example code for it please share with me and I am using CPU1 to access internal flash of 256KW.

Thanks,

Sid C