Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE, MOTORWARE
I ran Sysconfig 1.15 standalone on my Mac computer. I installed the latest C2000ware version 4.03 in Sysconfig so I could use some of the newer features. In Code Composer Studio I can't seem to get Sysconfig to run anything past 4.02.
When I copy my sysconfig file to the project, I get the following error and many more similar errors

When I launch Sysconfig in Code Composer I get the following dialog showing that the latest version of C2000Ware is 4.02, not 4.03. The instructions say to browse to the latest C2000ware but there is no button or way to browse (as there is in the standalone version). If I hit the big browse button it only lets me select .syscfg files.

In the standalone version there is a browse button:

I made sure that I am using the latest products in Code Composer Studio:

How can I use my Sysconfig file that I created in the standalone version in my project?
Regards