Part Number: TMS320F28377S
Other Parts Discussed in Thread: TMS320F28379S
1.Analyzing System Loading with RTOS Analyzer:
Problem 1:
when the CCS is on debug over 10 seconds, the CCS will interrupt by itself .
The “Records” in “ROV” has nothing and show message below.

Problem 2:
when the CCS is on debug less than 10 seconds, the I hold the debugging button by myself.
The “Records” in “ROV” has some records,but there is nothing in the “CPU Load” /“Task Load”/ “CPU Load:Summary ” /“CPU Load:Details” /“Task Load:Summary ”“Task Load:Details”.
See debugging results bellow:




- The version is as bellow :
|
CCS |
CCS v11.1.0.00011 |
|
Compiler |
C2000 Compiler v21.12.0.STS |
|
XDCtools |
XDCtools v3.62.1.16.core |
|
SYS/BIOS |
SYS/BIOS v6.83.0.18 |
|
UIA |
uia_2_30_01_02 |
|
Target |
ti.targets.C28_float |
|
Platform |
ti.platforms.tms320x28:TMS320F28379S |
- The UIA Logging Configuration is as follow: