Part Number: TMS320F280037
Other Parts Discussed in Thread: C2000WARE
Hi team,
//#############################################################################
//
// FILE: i2c_ex1_loopback.c
//
// TITLE: I2C Digital Loopback with FIFO Interrupts
//
//! \addtogroup driver_example_list
//! <h1>I2C Digital Loopback with FIFO Interrupts</h1>
//!
//! This program uses the internal loopback test mode of the I2C module. Both
//! the TX and RX I2C FIFOs and their interrupts are used. The pinmux and I2C
//! initialization is done through the sysconfig file.
//!
//! A stream of data is sent and then compared to the received stream.
//! The sent data looks like this: \n
//! 0000 0001 \n
//! 0001 0002 \n
//! 0002 0003 \n
//! .... \n
//! 00FE 00FF \n
//! 00FF 0000 \n
//! etc.. \n
//! This pattern is repeated forever.
//!
//! \b External \b Connections \n
//! - None
//!
//! \b Watch \b Variables \n
//! - \b sData - Data to send
//! - \b rData - Received data
//! - \b rDataPoint - Used to keep track of the last position in the receive
//! stream for error checking
//!
//
//#############################################################################
//
//
// $Copyright:
// Copyright (C) 2023 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "board.h"
//
// Defines
//
#define TARGET_ADDRESS 0x50
//
// Globals
//
uint16_t sData[2]; // Send data buffer
uint16_t rData[100]; // Receive data buffer
uint16_t rDataPoint = 0; // To keep track of where we are in the
// data stream to check received data
//
// Function Prototypes
//
__interrupt void i2cFIFOISR(void);
void Cla_delayus(int k)
{
int32_t i,m,j;
k = k;
for(i = 0; i<k; i++)
{
for(m=0;m<10;m++)
{
j++;
}
}
}
void main(void)
{
uint16_t i;
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Board initialization
//
Board_init();
GPIO_setPinConfig(GPIO_39_GPIO39);
GPIO_setPadConfig(39, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(39, GPIO_QUAL_ASYNC);
GPIO_setDirectionMode(39, GPIO_DIR_MODE_OUT);
GPIO_setPinConfig(GPIO_42_I2CA_SDA);
GPIO_setPadConfig(42, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(42, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(GPIO_43_I2CA_SCL);
GPIO_setPadConfig(43, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(43, GPIO_QUAL_ASYNC);
GPIO_setPinConfig(GPIO_45_GPIO45);
GPIO_setPadConfig(45, GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(45, GPIO_QUAL_ASYNC);
GPIO_setDirectionMode(45, GPIO_DIR_MODE_OUT);
// For loopback mode only
//
// I2C_setOwnAddress(I2CA_BASE, TARGET_ADDRESS);
I2C_disableModule(I2CA_BASE);
I2C_initController(I2CA_BASE, DEVICE_SYSCLK_FREQ, 400000, I2C_DUTYCYCLE_50);
I2C_setTargetAddress(I2CA_BASE, 0x50);
// I2C_enableLoopback(I2CA_BASE);
I2C_setOwnAddress(I2CA_BASE, 0);
I2C_setBitCount(I2CA_BASE, I2C_BITCOUNT_8);
I2C_setAddressMode(I2CA_BASE, I2C_ADDR_MODE_7BITS);
// I2C_enableFIFO(I2CA_BASE);
// I2C_clearInterruptStatus(I2CA_BASE, I2C_INT_RXFF | I2C_INT_TXFF);
// I2C_setFIFOInterruptLevel(I2CA_BASE, I2C_FIFO_TX1, I2C_FIFO_RX2);
// I2C_enableInterrupt(I2CA_BASE, I2C_INT_RXFF | I2C_INT_TXFF);
I2C_setEmulationMode(I2CA_BASE, I2C_EMULATION_FREE_RUN);
I2C_enableModule(I2CA_BASE);
// Interrupts that are used in this example are re-mapped to ISR functions
// found within this file.
//
// Interrupt_register(INT_I2CA_FIFO, &i2cFIFOISR);
GPIO_writePin(45,1);
// Initialize the data buffers
//
GPIO_writePin(39,0);
for(i = 0; i < 2; i++)
{
sData[i] = i;
rData[i]= 0;
}
//
// Enable interrupts required for this example
//
// Interrupt_enable(INT_I2CA_FIFO);
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
while(1)
{
GPIO_writePin(45,0);
I2C_setTargetAddress(I2CA_BASE, 0x50);
I2C_setConfig(I2CA_BASE, I2C_CONTROLLER_SEND_MODE);
I2C_setDataCount(I2CA_BASE, (100 + 2));
I2C_putData(I2CA_BASE, 0);
I2C_putData(I2CA_BASE, 1);//地址0x0001
I2C_sendStartCondition(I2CA_BASE);
for(i=0;i<100;i++)
{
Cla_delayus(15);
I2C_putData(I2CA_BASE,i);
}
Cla_delayus(50);
GPIO_writePin(45,1);
I2C_sendStopCondition(I2CA_BASE);
Cla_delayus(1000);
while(I2C_isBusBusy(I2CA_BASE));
I2C_setTargetAddress(I2CA_BASE, 0x50);
I2C_setDataCount(I2CA_BASE, 2);
I2C_putData(I2CA_BASE, 0);
I2C_putData(I2CA_BASE, 1);//地址0x0001
I2C_setConfig(I2CA_BASE, I2C_CONTROLLER_SEND_MODE);
I2C_sendStartCondition(I2CA_BASE);
Cla_delayus(20);
I2C_setDataCount(I2CA_BASE, 100);
I2C_setConfig(I2CA_BASE, I2C_CONTROLLER_RECEIVE_MODE);
rData[0] = I2C_getData(I2CA_BASE);
I2C_sendStartCondition(I2CA_BASE);
for(i=1;i<100;i++)
{
Cla_delayus(15);
rData[i] = I2C_getData(I2CA_BASE);
}
I2C_sendStopCondition(I2CA_BASE);
Cla_delayus(30000);
}
}
Changing the above program from the I2C_ex2_EEPROM.c routine will get stuck in the following statement when written:
While(I2C_isBusBusbusy(I2C_base));
Always busy.
Also, the read has always failed. The actual application cannot use interrupts in the routine due to logical relationships and the customer can only poll for writes.
1) Why is the busy state still present after the transmission is complete and cannot be cleared?
2) What is the correct read logic? In current writing, only the clock for the byte of the address is written, and the clock for reading is completely out.
Could you help check this case? Thanks.
Best Regards,
Cherry