Other Parts Discussed in Thread: DRV8305,
Hi,
I am using TMS320F28027F and DRV8305 for development of sensorless BLDC Controller. My application requires motor to run in clockwise / counter-clockwise direction with max RPM 150000. I have checked BLDC motor specifications and it is capable to run upto 150000.
In USER.H for user IQ FULL SCALE FREQ I have entered value 1300 so motor can rotate upto 78000.
#define USER_IQ_FULL_SCALE_FREQ_Hz (1300.0)
But to run at 150000 I need to increase that value. What is the maximum value that can be written for USER_IQ_FULL_SCALE_FREQ_Hz .
After increasing user full scale frequency value will motor run at 150000 rpm?
Thank you
Vaishali