Part Number: TMS320F28386D
Hi,
I want to implement the bootloader and application concept in CPU1. Below is the flash layout.
1) bootloader : BEGIN => flash 0(0x80000), code => flash 4
2) application : BEGIN => flash 13(0xBE000), code => flash 6
I flashed the application image into CPU1 first, then debug the bootloader flash image. In the bootloader code, I want to jump to Application with below command.
__asm(" LCR #0xBE000");
But, I always got illegal instruction trap when I want to step over this instruction in CCS.
In the map file of application image, I have below item:
0009b424 00000008 f2838x_codestartbranch.obj (.text)
I also checked the data in address 0xBE000, it's 0x0049b424, seems correct.
What's wrong with my implementation? Do you have any suggestions?