This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: Stack size and realtime monitor

Expert 2480 points

Part Number: TMS320F28386D

One question: One project without RTOS, where I can check the stack size for this project?

Onther question: Do CCS support the real time monitor the stack usage status ?

  • Hello,

    You can view the stack size using the Memory Allocation view and clicking the drop-down arrow on the memory where the .stack section is made:

    Alternatively, you can check the linker command file to modify the size allocated for stack.

    Onther question: Do CCS support the real time monitor the stack usage status ?

    I do not believe there is any tool for this, I will forward this question to the CCS team to see if there is anything.

    Best regards,

    Omer Amir

  • I do not believe there is any tool for this, I will forward this question to the CCS team to see if there is anything.

    Usually such functionality is available when using an RTOS. The associated RTOS tools often have a tool to monitor the stack usage. For non-RTOS applications, CCS does not have any out-of-the-box tools for this.