Other Parts Discussed in Thread: TMS320F28027
Hi There
Slight confusion on the SPI SPISTE-bar pin on the TMS320F28027 device.
I would have thought as a master device it would want to connect to multiple slave devices, yet the SPI manual indicates that the SPISTE-bar pin is used for chip select in master as well as slave modes (I had assumed a GPIO pin would be used per slave device)
Is my understanding correct? can I only connect one SPI slave to the controller?
Thanks