Part Number: TMS320F28377S
We're designing a new board based on the TMS320F28377S and are considering adding external RAM for the purpose of debugging our application from RAM instead of from on-board FLASH. The incentive being that we will have faster downloads and unlimited break points.
Questions:
1) Is it possible from Code Composer to download code directly to an external RAM and run?
2) Is it true that the number of breakpoints is essentially unlimited?
3) Are there any limitations on above with respect to the type of external RAM used (DRAM vs SRAM) ?
Thanks in advance,
Paul Hetherington
Note that we're porting our code from and existing project (28335) and know that the 377 on-board RAM is not large enough for this code.