This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Locked Flash

Hello all,

 

I had a problem when flasing my 28335 board, during the erase process CCSv4 froze and the operation ended, now the the controller is locked and it can't be acces to program again. Before this problem I downloaded and programed the flash several time succesfully. Is there a problem with CCSv4? Im using version 4.2.3.00004 with C2000 Code Generation Tools 6.0.1 and all the latest updates.

 

Is there a problem with the real time mode? Just before the download that damaged the controller I was running in real time mode. Before downloading the code I stoped the real time mode, stoped the debugging and then started a new debugging of the active project.

 

Thanks,

 

Maziel

  • Hi Maziel,

    Probably your FLASH is only depleted. Did you try a depletion recovery in CCSV4?? Tools->On Chip Flash -> Depletion Recovery.

    Concerning the reason of your problem - was your power source stable while you were flashing the target? Your procedure before flashing as you describe it was correct. I don't think that CCSV4 has a systematic problem with flashing, otherwise this forum would be flooded with problem reports.

    Best regards

    Andreas

  • Hi Andreas,

    Thank you for your response. The power supply was stable during the flashing, is a power supply + UPS system. 

     

    I did try the depletion recovery and it couldn't be initiated, an error appears in CCS.

    Another thing that happened in a different occasion was that during the stop debugging step, CCS froze and it killed my computer, the Blue Screen of Death appeared and have to shut down the pc.

    Since then I have returned to CCS v3.3 so i do not damage another board. But my system is windows 7 and sometimes CCSv3.3 freezes.

    Any suggestions?

    What would happen if you dont stop the real time mode and attempt to start the debugging process?

    Thanks,

    Maziel