Part Number: TMS320F28379D
Hi,
Can I run two Teknic 2310P PMSM engines independently using the TMS320F28379D launchpad? Dual motor control examples are available. But this structure is back to back connection (connecting one motor to another as a load). But I want to independently control the position of two motors operating on two axes. Is it possible? Can I install programs on CPU1 and CPU2 separately? Or is there another way to do this.