Part Number: TMS320F28334
Other Parts Discussed in Thread: TMS320F28379S, TMS320F28075
Hi Experts,
I am trying to help one of our customers. Their company is currently working on a new project and they are considering upgrading the current Digital Signal Processor (DSP) on our controller board for Permanent Magnet Synchronous Motor (PMSM) control.
Their current DSP is TMS320F2833. They want at least the specification of this chip, ideally better.
Here are the minimum specifications that DSP has to fulfill:
- 150 MHZ
- 256K x 16 flash, 34K x 16 SARAM
- 9 x ADC
- CANbus Tx Rx module
- 12 x EPWM
- External Memory Interface (EMIF) for communicating with FPGA
- SPI
- 12 x GPIO
The above is a must and they are looking for a possible upgrade to a more powerful DSP that can do the PMSM control. I have filter a list of devices but was not sure what is best to suggest. May I ask for your assistance on this so that our customer can proceed with their design accordingly? Thank you so much in advance.
Best regards,
Gerald