Part Number: TMS320F280039C
Dear champs,
I am asking this for our customer.
The user has the same problem like
"
When I write DEVICE_DELAY_US(100), the timing is correct.
When I define any type of variable UINT16_t, float, long double and call DEVICE_DELAY_US(variable) the timing is wrong.
Looking at it
#define DEVICE_DELAY_US(x) SysCtl_delay(((((long double)(x)) / (1000000.0L / \
(long double)DEVICE_SYSCLK_FREQ)) - 9.0L) / 5.0L)
So, shouldn't whatever data type I input be converted to long double?
The timing always goes to ~2.4x 100 when I type to use any data type as input.
"
But it's not clear what the solution is in that post.
Do you have any suggestion if the user wants to use variable as a delay during runtime?
That is, the user just wants to delay 2.5us, 4 us, 6 us, like that during run time.
But these delay time are variables.
Can they use DEVICE_DELAY_US(var)?
Any suggestion here?