Hi
I want to run the usb_bulk_example application on a F28069 controlCard together with the usb_bulk_example console PC program.
I installed and loaded all the necessary programs:
- usb device driver (usb_dev_bulk.inf) on a PC
- Console application (usb_bulkexample.exe) on a PC
- usb_dev_bulk project on CCS4.2
I loaded the F28069 application to the controlCard. The program runs but the USB signals were on the bus for a few seconds and then Windows told me with a small yellow message:
USB DEVICE NOT RECOGNIZED...
Additional the Windows device manager shows a yellow exclamation point at the "Generic Bulk Device" entry
any ideas ?
Mike