Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
how to down load code 1 time for multi core DSP like 28388d.
currently I can only down load code 1 by 1, it is not efficiency.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
how to down load code 1 time for multi core DSP like 28388d.
currently I can only down load code 1 by 1, it is not efficiency.
Could you kindly provide more clarification on your query?
Do you mean how to download example code (like C2000ware)? Or do you mean flashing the program to the dsp, that will ultimately run on the microcontroller?
Thanks.
Hi Sahil
currently I can build the code with CCS for cpu1 and cpu2 in the F28388D core. But I can only burn the code via debug page .
1st burn the cpu1 and then cpu2.
so is there any steps can burn the cpu1 and cpu2 simultaneously。
Hi,
You can go to Run -> Debug Configurations.
After choosing the appropriate ccxml file, on the right hand side, select the Program pane as shown below:

Here you can choose the project to be loaded on either CPU (use the device drop down to select between CPU1 and CPU2). Click Debug.
Consequently, everytime you click debug, CPU1 and CPU2 will be burned simultaneously.
Thanks.