Part Number: LAUNCHXL-F2800137
Other Parts Discussed in Thread: C2000WARE, , BOOSTXL-DRV8323RS
Hi Team,
Here's an issue from the customer may need your help:
from【C2000Ware_MotorControl_SDK_4_02_01_00】
use LAUNCHXL-F2800137 + BOOSTXL-DRV8323RS
CCS 12.1.0.00007
I am currently testing the Level 1~Level 4 Incremental Build project.
When I want to use the [DATALOG module] to display the current current value,
but a lot of errors occur after compiling.
I would like to ask if the error is caused By the fact that the F280013x series does not have the DMA function?
If yes, then I want to use [DATALOG module] on F280013x, how to achieve it?


--
Thanks & Regards
Yale