This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: On-Chip temperature limit

Part Number: TMS320F28069


Dear Experts,

I would like to inquire about the operating temperature limit of TMS320F28069PZP. I utilize the internal temperature sensor on Channel A5 to monitor on-Chip temperature. In our application, the chip temperature can reach up to 122 degrees Celsius. At this point, the MCU is still running normally and performing its function.

However, as shown in the datasheet, the temperature limit for this chip is 125 degrees Celsius. I am concerned about what might happen if the chip temperature exceeds the operating limit. Will it crash? Should we be worried about this and apply thermal cooling measures, such as a heatsink or thermal pad?

Best regards,
Luiz