Other Parts Discussed in Thread: TMS320F28377S
TI support hello.
I am working with the TMS320F2812 and have a problem during power up..
i am booting from flash and it seems that the MCU do not work after power up.
if i close power and open - the MCU work.
it look like the power sequence is ok (first 3.3v than 1.8v and than reset).
when "cold start" 1.8v start from 0v and MCU do not run.
when closing power (close , wait several second and reopen) 1.8v not starting from zero.
it start from 0.4v and MCU run (for second powering up)
for test I connected resistor from 1.8v to GND (dump voltage in order to start second power up from 0v not 0.4v) and MCU did not rum.
(remove resistor and MCU run for second power up).
MCU run as well in debug mode.
can you assist?
Yehoram