Part Number: DRV8301
Other Parts Discussed in Thread: BOOSTXL-DRV8320RS, LAUNCHXL-F280049C, TMDSCNCD280049C, C2000WARE, , MOTORWARE, DRV8320
Hello,
I have been evaluating a combination of the BOOSTXL-DRV8320RS and the LAUNCHXL-F280049C, and have been quite happy with the results.
However I am interested in evaluating the F280049C on the higher power DRV8301-HC-EVM Rev D. To that end, I have a setup described by option 1 in this post:
"1. DRV8301-HC-C2-KIT + TMDSCNCD280049C"
I have the DRV8301-HC-EVM Rev D, a DIMM adapter board and the TMDSCNCD280049C.
It appears there are two paths in the Motor Control SDK for instaSPIN-FOC for this board, and pieces are missing from both:
Path 1:
InstaSPIN-FOC Labs contained in the C2000Ware_MotorControl_SDK_4_01_00_00
These labs support the BOOSTXL-DRV8320RS + LAUNCHXL-F280049C configuration as before just fine, however it appears there at some point was an intention to also allow support of the DRV8301.
The F280049C lab guide at "...\C2000Ware_MotorControl_SDK_4_01_00_00\solutions\common\sensorless_foc\docs\labs\MotorControl SDK InstaSPIN Lab Guide.pdf" describes the labs as compatible with
something called an HV kit:
The following figure is a code snippet from "labs.h" also appears drivers for the DRV8301 board may have been implemented:

However, no such 'drv8301.h' drivers exists anywhere I could search.
PATH 2:
InstaSPIN-FOC labs contained in "...\motorware_1_01_00_18\sw\solutions\instaspin_foc\boards\drv8301kit_revD\f28x\"
These labs are all in support directly of the DRV8301-HC-EVM Rev D (considering the path above alone).
The F2802x, F2805x, and F2806x are supported, but there is a lack of support for the F280049C board in these labs:
I am less familiar with these labs. It appears that these labs have perhaps fallen out of favor compared to the MotorControl SDK, which more directly supports the F280049C that I would prefer to implement in my design.
A solution would be to purchase the TMDSCNCD28069MISO chip, the F2806x supported variant.
I feel like I am really close to running the DRV8301-HC-EVM Rev D with either the missing drivers for the DRV8301, or some slight modifications to the code for the F2806x supported lab.
Do drivers for the DRV8301 exist?
Could modifications could be made, for example to the F2806x lab, to support the TMDSCNCD280049C?
Am I better off using the TMDSCNCD28069MISO for this purpose?
The post I linked above claimed the MotorControl SDK would have example lab projects for the DRV8301-HC-EVM Rev D + TMDSCNCD280049C, but only the MotorWare SDK has any labs for the DRV8301.
Any further insight into my options would be much appreciated.