This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: external build-environment / CMAKE

Part Number: TMS320F280039C


Hi team,

I want to ask you, if TI supports an external build environment (like CMAKE) for its C2000-processors (e.g. F280049C/F280039C).

If there is no example currently available,  I would like to clarify, if CCS has some built-in features, which are required for C2000-build on the one hand, that cannot be performed without CCS on the other hand.

In other words: Are there any blocking points already well known preventing a CMAKE build).

Thanks and best regards

Jens