Hi,
I am working on a 29379D system which is connected through SPI and Serial comm to a Sitara ARM processor running an OS. Is there any way to run an firmware upgrade to 28379D through the ARM processor? , I can see that there is a serial flash programming solution for the 28379D through SCI-A as given in SPRAAL3 document but is it possible to do that through another processor if it is connected to the SCI interface?
The objective is to be able to send the required file to the ARM processor from a PC and then pass it from the ARM processor to the 28379D for the firmware update. Is there a possibility that this can be done or it is much easier to have access to the serial port of the 28379D separately and load the out file directly from the PC through a JTAG tool. Any suggestions or direction to documentation that I can read would be really helpful.
Thank you,
Aditya