Part Number: TMS320F280049
Dear Champs,
I am asking this for our customer.
In this post,
Manoj said,
"You don't need to be a clock master to use clock control feature. From a hardware perspective, you need to route AMC1303M Clock signal to SD-C1 (Filter channel 1 clock). This clock can then be used internally to all the other 3 filter channels (2 / 3 / 4)."
Because the user has limited usable pins, they want to use as few clock pin as possible for SDFM.
Would you please confirm?
On 100-pin F280049, is the internal clock sharing also valid? That is, the user can use single pin for clocking SD1-CK1 and all other SD1-CK2/3/4 share the same clocking SD1-CK1?
Is our understanding correct?