Part Number: TIDM-02002
Other Parts Discussed in Thread: C2000WARE, TMS320F28377D, TMS320F28379D, POWERSUITE, SYSCONFIG, SFRA
Hello, I have a syscfg project imported from C2000Ware, specifically the TIDM-02002. This is natively targeted to F28004x family, and I would like to "convert" it to F28377D.
To do this, I've opened the device view in the syscfg editor and I've used the "Switch" command. Several options are available:

Unfortunately all options work ok except for the one I need, i.e. TMS320F28377D. If I choose this option and then save, an error pops out:

I have two questions:
1) Is there a way to fix the TMS320F28377D migration? It seems that one file is just missing: note in the dropdown menu how the 377D option ends with a .xml, as if CCS did not find the respective configuration file.
2) If not, can I get around this issue just by selecting TMS320F28379D (which is almost identical, apart from the CLB support) and perhaps by changing the target config file to TMS320F28377D just to make sure that the debugger does not complain?
Thank you!
L.