Part Number: C2000WARE
Other Parts Discussed in Thread: CCSTUDIO,
Hi Experts,
Good day.
We are using the F2837 family of C2000 and for that to be developed we are setting up a Docker toolchain with CCStudio 12.3 and CCWare 4.03. On Ubuntu Linux image. The problem is that both installations of CCStudio and C2000ware complete, but CCstudio does not find the C2000ware installation while building the project. all path and setting seem correct.
Building...
Buildfile generation error occurred..
Product c2000ware_software_package v4.3.0.00 is not currently installed and no compatible version is available. Please install this product or a compatible version.
Build stopped..
This is a screenshot from Docker Container. Ubuntu 22.04, ccs12.3, and CCWare 4.03.
Please advise.
Reards,
Josel