Part Number: TMS320F28035
Hello,
In the application note "Digital Peak Current Mode Control With Slope Compensation Using the TMS320F2803x"
https://www.ti.com/lit/an/sprabe7a/sprabe7a.pdf
there's some discussion on p.20 about comparing the measured and simulated results. The app note says:
"The gain plot at low frequencies is less than the modeled result. This is due to the combination of the way
in which the frequency response is measured and the discrete time nature of the controller. When the
frequency of the injected signal is low, the input to the discrete time controller does not significantly
change from cycle to cycle and the response cannot be accurately measured."
Wondering if you can point me to additional resources explaining this low frequency measurement phenomenon? I'm looking for a bit more support to better understand it and convince colleagues.
Thanks!