Part Number: TMS320F28377D-EP
Other Parts Discussed in Thread: C2000WARE
Hello,
I see on the datasheet that the maximum SYSCLK TMS320F28377D-EP is 200 MHz. The datasheet also lists the frequency range for the external crystal as 10 - 20 MHz. Does the frequency of the external crystal have any effect on how fast code can execute, or that entirely determined by SYSCLK? For example, would using a 20 MHz crystal instead of a 10 MHz make the same code execute faster?
Thanks,
Kevin