This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28379D: Generating 450KHz PWM Sine Wave

Part Number: TMDSCNCD28379D

Hello TI Team, In one of my product I want to generate 400KHz sine wave using ePWM module with at least 20 data points of carrier which will be modulated based on Sine table for 0 to 360 degree angle. Wanted to know if it is possible to do using C2000 series of microcontroller as the carrier frequency for 20 data points will be around 8 MHz? If it is feasible to do then can you please share any application note where such example is given ?

Thanks!