This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Performance issue between executing code in RAM and flash.

I am testing 28035 Picolo.  I found out something strange regarding execution code in RAM and Flash. I used GPIO toggle example code to test the performance of code execution in RAM and Flash and execution code in RAM is three or four times faster than the execution code in Flash. I reduced from two to one the wait cycle in InitFlash function to get the max performance but this did not make any improvement in performance.  Is there any way to expedite the code execution time like enable the prefetch?

Thanks in advance.

Best regards,

Thomas.