Hello,
Now I is using CCS V3.3. I want to Include header file into Assembly . But arised many Error.
For example: In Assembly source
.cdecls C,LIST, "DSP2802x_EPWM_defines.h"
This DSP2802x_EPWM_defines file is consist of : Structure, Union,..... ect.
such as:
struct TBCTL_BITS { // bits description
Uint16 CTRMODE:2; // 1:0 Counter Mode
Uint16 PHSEN:1; // 2 Phase load enable
Uint16 PRDLD:1; // 3 Active period load
Uint16 SYNCOSEL:2; // 5:4 Sync output select
Uint16 SWFSYNC:1; // 6 Software force sync pulse
Uint16 HSPCLKDIV:3; // 9:7 High speed time pre-scale
Uint16 CLKDIV:3; // 12:10 Timebase clock pre-scale
Uint16 PHSDIR:1; // 13 Phase Direction
Uint16 FREE_SOFT:2; // 15:14 Emulation mode
};
union TBCTL_REG {
Uint16 all;
struct TBCTL_BITS bit;
};
--------------------------------------------------------------------------------------------------------------------
I want to use above structure and union in Assembly. But Can not completed.
Could you tell me about this problem?