Part Number: C2000-GANG
Hi Team,
There's an issue from the customer need your help:
It’s okay to burn two devices individually, but you can’t burn both at the same time. If both are connected at the same time, only one of them can be burned. The other host computer shows that it is not connected.
At present, there are two dsp chips of the same type on the driver board. The power supply and GND of the two are connected. The same program is burned. Now the burning can not be achieved at the same time and it is very unstable. Sometimes it can be burned and sometimes it can’t. No guidance on how to wire and configure the upper computer. I have read the user manual and have not solved it. I want to know whether the two chips are connected to the programmer alone or the two signal lines are connected in series. Also, see the manual for connecting the programmer. The Vext pin of the power supply should have an output voltage of 3.3V, but there is no voltage output after measurement. Is this normal?
This is a self-test report. There is no error before the connection, and an error is reported after the connection. The 3.3V of the chip is connected to the vext pin of the programmer, and the chip also has a separate power supply. The TMS, TDI, TDO, TCK, and TRST pins of the two chips are connected separately. The respective pins of the two channels of the programmer, the GND of the chip and the GND of the programmer are not connected. (In addition, I tried to connect the GND, but it is also invalid. I also tried that the chip is not powered separately, and the host computer reports an error VCC is low)
=== C2000-GANG Self test results ( Saturday, April 22, 2023, 11:27:27 ) ===
Adapter SN ------: 21111617
Hardware --------: C2K : 01.05
Access key ------: C2000 - Gang Programmer
Silicon Number --: 12F0 5B51 2700 0700
API Firmware ----: C2K-Gang AC28: 01.01.09.00
BOOT Firmware ---: G430BOOT B430: 01.00.02.00
GUI Software ----: C2000-Gang-GUI G28x: 01.01.09.00
DLL Software ----: C2000-Gang-DLL D280: 01.01.09.00
================ Test results =============
No. name parameter limits result status
1: Data Bus (ALL LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK <<
2: Data Bus (ALL HIGH) 0x00FF (0xFFFF - 0xFFFF) Result: 0xFFFF ... >> OK <<
3: Data Bus (D-0 HI ) 0x0001 (0x0101 - 0x0101) Result: 0x0101 ... >> OK <<
4: Data Bus (D-1 HI ) 0x0002 (0x0202 - 0x0202) Result: 0x0202 ... >> OK <<
5: Data Bus (D-2 HI ) 0x0004 (0x0404 - 0x0404) Result: 0x0404 ... >> OK <<
6: Data Bus (D-3 HI ) 0x0008 (0x0808 - 0x0808) Result: 0x0808 ... >> OK <<
7: Data Bus (D-4 HI ) 0x0010 (0x1010 - 0x1010) Result: 0x1010 ... >> OK <<
8: Data Bus (D-5 HI ) 0x0020 (0x2020 - 0x2020) Result: 0x2020 ... >> OK <<
9: Data Bus (D-6 HI ) 0x0040 (0x4040 - 0x4040) Result: 0x4040 ... >> OK <<
10: Data Bus (D-7 HI ) 0x0080 (0x8080 - 0x8080) Result: 0x8080 ... >> OK <<
11: Data-2 Bus (ALL LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK <<
12: Data-2 Bus (ALL HIGH) 0x00FF (0xFFFF - 0xFFFF) Result: 0xFFFF ... >> OK <<
13: Data-2 Bus (D2-0 HI ) 0x0001 (0x0101 - 0x0101) Result: 0x0101 ... >> OK <<
14: Data-2 Bus (D2-1 HI ) 0x0002 (0x0202 - 0x0202) Result: 0x0202 ... >> OK <<
15: Data-2 Bus (D2-2 HI ) 0x0004 (0x0404 - 0x0404) Result: 0x0404 ... >> OK <<
16: Data-2 Bus (D2-3 HI ) 0x0008 (0x0808 - 0x0808) Result: 0x0808 ... >> OK <<
17: Data-2 Bus (D2-4 HI ) 0x0010 (0x1010 - 0x1010) Result: 0x1010 ... >> OK <<
18: Data-2 Bus (D2-5 HI ) 0x0020 (0x2020 - 0x2020) Result: 0x2020 ... >> OK <<
19: Data-2 Bus (D2-6 HI ) 0x0040 (0x4040 - 0x4040) Result: 0x4040 ... >> OK <<
20: Data-2 Bus (D2-7 HI ) 0x0080 (0x8080 - 0x8080) Result: 0x8080 ... >> OK <<
21: Vcc Target-1 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.02 V ... >> OK <<
22: Vcc Target-2 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK <<
23: Vcc Target-3 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK <<
24: Vcc Target-4 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK <<
25: Vcc Target-5 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK <<
26: Vcc Target-6 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.01 V ... >> OK <<
27: Vcc Target-7 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 2.42 V ... >> ERROR <<
28: Vcc Target-8 (ALL OFF) 0.00 V ( 0.00 to 0.30) Result: 0.02 V ... >> OK <<
29: Translators VT (OFF) 0.00 V ( 0.00 to 0.50) Result: 0.02 V ... >> OK <<
30: Translators VT (ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.29 V ... >> OK <<
31: Vpp Voltage-in 10.00 V ( 8.00 to 12.00) Result: 10.43 V ... >> OK <<
32: Vpp Voltage 7.00 V ( 6.50 to 7.30) Result: 6.87 V ... >> OK <<
33: Internal Vcc-3.3V 3.30 V ( 3.20 to 3.40) Result: 3.30 V ... >> OK <<
34: Vcc Target-1 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.29 V ... >> OK <<
35: Vcc Target-2 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.30 V ... >> OK <<
36: Vcc Target-3 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.30 V ... >> OK <<
37: Vcc Target-4 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.33 V ... >> OK <<
38: Vcc Target-5 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.31 V ... >> OK <<
39: Vcc Target-6 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.33 V ... >> OK <<
40: Vcc Target-7 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.30 V ... >> OK <<
41: Vcc Target-8 (ALL ON 3.3V) 3.30 V ( 3.10 to 3.50) Result: 3.32 V ... >> OK <<
42: Vcc discharge (250ms)Target-1 3.30 V ( 0.30 to 1.50) Result: 0.79 V ... >> OK <<
43: Vcc discharge (250ms)Target-2 3.30 V ( 0.30 to 1.50) Result: 0.79 V ... >> OK <<
44: Vcc discharge (250ms)Target-3 3.30 V ( 0.30 to 1.50) Result: 0.78 V ... >> OK <<
45: Vcc discharge (250ms)Target-4 3.30 V ( 0.30 to 1.50) Result: 0.79 V ... >> OK <<
46: Vcc discharge (250ms)Target-5 3.30 V ( 0.30 to 1.50) Result: 0.79 V ... >> OK <<
47: Vcc discharge (250ms)Target-6 3.30 V ( 0.30 to 1.50) Result: 0.78 V ... >> OK <<
48: Vcc discharge (250ms)Target-7 3.30 V ( 0.30 to 1.50) Result: 2.44 V ... >> ERROR <<
49: Vcc discharge (250ms)Target-8 3.30 V ( 0.30 to 1.50) Result: 0.79 V ... >> OK <<
50: Vcc Target-1 ( #1 ON ) 0.00 V ( 3.10 to 3.50) Result: 3.29 V ... >> OK <<
51: Vcc Target-2 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
52: Vcc Target-3 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
53: Vcc Target-4 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
54: Vcc Target-5 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
55: Vcc Target-6 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.15 V ... >> OK <<
56: Vcc Target-7 ( #1 ON ) 0.00 V ( 0.00 to 0.50) Result: 2.44 V ... >> ERROR <<
57: Vcc Target-8 ( #1 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
58: Vcc Target-1 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
59: Vcc Target-2 ( #2 ON ) 0.00 V ( 3.10 to 3.50) Result: 3.30 V ... >> OK <<
60: Vcc Target-3 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
61: Vcc Target-4 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
62: Vcc Target-5 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
63: Vcc Target-6 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.15 V ... >> OK <<
64: Vcc Target-7 ( #2 ON ) 0.00 V ( 0.00 to 0.50) Result: 2.44 V ... >> ERROR <<
65: Vcc Target-8 ( #2 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
66: Vcc Target-1 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
67: Vcc Target-2 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
68: Vcc Target-3 ( #3 ON ) 0.00 V ( 3.10 to 3.50) Result: 3.29 V ... >> OK <<
69: Vcc Target-4 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
70: Vcc Target-5 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
71: Vcc Target-6 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.15 V ... >> OK <<
72: Vcc Target-7 ( #3 ON ) 0.00 V ( 0.00 to 0.50) Result: 2.44 V ... >> ERROR <<
73: Vcc Target-8 ( #3 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
74: Vcc Target-1 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
75: Vcc Target-2 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
76: Vcc Target-3 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
77: Vcc Target-4 ( #4 ON ) 0.00 V ( 3.10 to 3.50) Result: 3.33 V ... >> OK <<
78: Vcc Target-5 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
79: Vcc Target-6 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.15 V ... >> OK <<
80: Vcc Target-7 ( #4 ON ) 0.00 V ( 0.00 to 0.50) Result: 2.44 V ... >> ERROR <<
81: Vcc Target-8 ( #4 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
82: Vcc Target-1 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
83: Vcc Target-2 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
84: Vcc Target-3 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
85: Vcc Target-4 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
86: Vcc Target-5 ( #5 ON ) 0.00 V ( 3.10 to 3.50) Result: 3.31 V ... >> OK <<
87: Vcc Target-6 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
88: Vcc Target-7 ( #5 ON ) 0.00 V ( 0.00 to 0.50) Result: 2.44 V ... >> ERROR <<
89: Vcc Target-8 ( #5 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
90: Vcc Target-1 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
91: Vcc Target-2 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
92: Vcc Target-3 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
93: Vcc Target-4 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
94: Vcc Target-5 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
95: Vcc Target-6 ( #6 ON ) 0.00 V ( 3.10 to 3.50) Result: 3.33 V ... >> OK <<
96: Vcc Target-7 ( #6 ON ) 0.00 V ( 0.00 to 0.50) Result: 2.44 V ... >> ERROR <<
97: Vcc Target-8 ( #6 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
98: Vcc Target-1 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
99: Vcc Target-2 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
100: Vcc Target-3 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
101: Vcc Target-4 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
102: Vcc Target-5 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
103: Vcc Target-6 ( #7 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
104: Vcc Target-7 ( #7 ON ) 0.00 V ( 3.10 to 3.50) Result: 3.29 V ... >> OK <<
105: Vcc Target-8 ( #7 ON ) 3.30 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
106: Vcc Target-1 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.17 V ... >> OK <<
107: Vcc Target-2 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
108: Vcc Target-3 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
109: Vcc Target-4 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
110: Vcc Target-5 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.16 V ... >> OK <<
111: Vcc Target-6 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 0.15 V ... >> OK <<
112: Vcc Target-7 ( #8 ON ) 0.00 V ( 0.00 to 0.50) Result: 2.44 V ... >> ERROR <<
113: Vcc Target-8 ( #8 ON ) 3.30 V ( 3.10 to 3.50) Result: 3.32 V ... >> OK <<
114: SD Power OFF 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK <<
115: SD Power ON 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK <<
116: SD Discharge - delay 2ms 0x0010 (0x0001 - 0x0001) Result: 0x01 ... >> OK <<
117: SD Discharge - delay 50ms 0x0010 (0x0000 - 0x0000) Result: 0x00 ... >> OK <<
118: BSL RX bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK <<
119: BSL RX bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK <<
120: BSL RX bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK <<
121: BSL RX bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK <<
122: BSL RX bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK <<
123: BSL RX bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK <<
124: BSL RX bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK <<
125: BSL RX bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK <<
126: BSL TX bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK <<
127: BSL TX bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK <<
128: BSL TX bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK <<
129: BSL TX bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK <<
130: BSL TX bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK <<
131: BSL TX bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK <<
132: BSL TX bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK <<
133: BSL TX bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK <<
134: TDI bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0xC4 ... >> ERROR <<
135: TDI bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x45 ... >> ERROR <<
136: TDI bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x46 ... >> ERROR <<
137: TDI bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x44 ... >> ERROR <<
138: TDI bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x4C ... >> ERROR <<
139: TDI bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x54 ... >> ERROR <<
140: TDI bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x64 ... >> ERROR <<
141: TDI bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x44 ... >> ERROR <<
142: TDIO Tx-bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x45 ... >> ERROR <<
143: TDIO Tx-bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x46 ... >> ERROR <<
144: TDIO Tx-bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x44 ... >> ERROR <<
145: TDIO Tx-bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x4C ... >> ERROR <<
146: TDIO Tx-bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x54 ... >> ERROR <<
147: TDIO Tx-bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x64 ... >> ERROR <<
148: TDIO Tx-bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x44 ... >> ERROR <<
149: TDIO Tx-bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0xC4 ... >> ERROR <<
150: TDIO Tx-Rx (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK <<
151: TDIO Tx-Rx (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK <<
152: TDIO Tx-Rx (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK <<
153: TDIO Tx-Rx (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK <<
154: TDIO Tx-Rx (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK <<
155: TDIO Tx-Rx (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK <<
156: TDIO Tx-Rx (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK <<
157: TDIO Tx-Rx (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK <<
158: TDIO Rx-bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x45 ... >> ERROR <<
159: TDIO Rx-bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x46 ... >> ERROR <<
160: TDIO Rx-bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x44 ... >> ERROR <<
161: TDIO Rx-bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x4C ... >> ERROR <<
162: TDIO Rx-bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x54 ... >> ERROR <<
163: TDIO Rx-bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x64 ... >> ERROR <<
164: TDIO Rx-bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x44 ... >> ERROR <<
165: TDIO Rx-bus (#84 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0xC4 ... >> ERROR <<
166: TMS bus (All HIGH) 0x00FF (0x00FF - 0x00FF) Result: 0xFF ... >> OK <<
167: TMS bus (All LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK <<
168: TMS bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x41 ... >> ERROR <<
169: TMS bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x42 ... >> ERROR <<
170: TMS bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK <<
171: TMS bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK <<
172: TMS bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK <<
173: TMS bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x60 ... >> ERROR <<
174: TMS bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x40 ... >> OK <<
175: TMS bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK <<
176: RST bus (All HIGH) 0x00FF (0x00FF - 0x00FF) Result: 0xFF ... >> OK <<
177: RST bus (All LOW) 0x0000 (0x0000 - 0x0000) Result: 0x00 ... >> OK <<
178: RST bus (#1 HIGH) 0x0001 (0x0001 - 0x0001) Result: 0x01 ... >> OK <<
179: RST bus (#2 HIGH) 0x0002 (0x0002 - 0x0002) Result: 0x02 ... >> OK <<
180: RST bus (#3 HIGH) 0x0004 (0x0004 - 0x0004) Result: 0x04 ... >> OK <<
181: RST bus (#4 HIGH) 0x0008 (0x0008 - 0x0008) Result: 0x08 ... >> OK <<
182: RST bus (#5 HIGH) 0x0010 (0x0010 - 0x0010) Result: 0x10 ... >> OK <<
183: RST bus (#6 HIGH) 0x0020 (0x0020 - 0x0020) Result: 0x20 ... >> OK <<
184: RST bus (#7 HIGH) 0x0040 (0x0040 - 0x0040) Result: 0x00 ... >> ERROR <<
185: RST bus (#8 HIGH) 0x0080 (0x0080 - 0x0080) Result: 0x80 ... >> OK <<
186: Keys buffer (All pull-up) 0x001F (0x001F - 0x001F) Result: 0x1F ... >> OK <<
187: Access to LCD RAM (0xAA) 0x00AA (0x00AA - 0x00AA) Result: 0xAA ... >> OK <<
188: Access to LCD RAM (0x99) 0x0099 (0x0099 - 0x0099) Result: 0x99 ... >> OK <<
189: Image Flash Access (get ID) 0x0002 (0x0001 - 0x0004) Result: 0x04 ... >> OK <<
============== Finished =================================
* Test failed!! 37 error(s).
=========================================================
Could you help check this case?
Thanks & Regards,
Ben