This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Ram error due to large program

Part Number: TMS320F28335

Hello all,

I am getting an error as in bellow:

<Linking>
"../28335_RAM_lnk.cmd", line 133: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment/blocking fails for section ".text" size 0x12f9 page 0. Available memory ranges:
RAML1 size: 0x1000 unused: 0x1000 max hole: 0x1000
error #10010: errors encountered during linking; "ADCEXT.out" not built

I think my ram memory is not large enough to put all the program in it. But how can i solve this? I am using the original file of 28335_RAM_lnk.cmd. Thank you all.