Hi,
I am using TMS320F2812 in my system with a SPI-based IC. This IC can work max 75Mbps SPI speed. F2812 SPI speed is limited such as given in the F2812 datasheet:
"Serial port performance is limited by I/O buffer switching speed. Internal prescalers must be adjusted such that the peripheral speed is less than the I/O buffer speed limit—20 MHz maximum." So,because of my applicaiton requirement, i have to switch another Microcontroller or ARM or DSP platform for higher IO speed than F2812. Can you help to find platform for higher IO speed?