Hi,
I am working on the design of an external charger for EV batteries. Specifically in case of DC fast charge: I need to know when the external charger communicates with EV BMS, what information about the EV battery is shared with the external charger. Min/Max current, Min/Max voltages, charging profile etc. so that the external charger can estimate battery SOC, define charging profile, know when to stop charging and the charging limits etc.
What standard I need to review to find the answer to the above questions. Or any helpful information is appreciated,
Thank you,
I was referred to this forum from below thread: