Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D
I am currently using CAN BUS of TMS320F28379D. However, this controller does not have ethernet port support. It is an excellent controller for Motor control and power electronics.
1. Is there any way to do the ethernet communication using external hardware (preferable Development kit) and TMS320F28379D?
I want to develop remote automation over TCP/IP protocol.
2. Any development board based solution is preferable like LAUNCHXL-F28379D Development kit.
Or
3. Any single compact development kit (Like STM32H743/753/742) for the solution of Motor control and power electronics with ethernet and CAN bus features?