Part Number: DRV8316REVM
Other Parts Discussed in Thread: DRV8316
Hey Guys,
Need some help with running the example code Universal_Motor_Control_Lab for the F280049c and DRV8316 devices there were some build errors earlier which were solved on this support link. Kevin Allen18
The code builds all fine but there was no motor movement seen, also do I need to make any changes to the expressions in the expressions window for this project similar to how we had to do for the example projects like IS07_Speed_Control (Changing the motorVars.flagEnableSys flag to 1 from 0). We even tried running the motor in a sensorless manner making tweaks to the code a bit, but we had no luck there as well, can you help us out with this one, have attached a code along this support request if you all want to have a look at the project files on your end.
FYI: This support request is in relation to the support request that was created earlier. I created this another request just because the problem explained there with the program not building because of the linking errors was resolved and i didn't want the other people referring to the forums getting confused with this question.... check out that post over here.
Thanks,
Shlok Desai