Part Number: TMS320F28386D
Hi,
We had a board which was perfectly working and were able to program the CPUs without issue but it started getting complicated and now totally impossible, the device won't connect at all.
We looked with the oscilloscope and we don't see anything on the TDO line.
Here is the log from the scan test:
[Start: Texas Instruments XDS2xx USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\x493146\AppData\Local\TEXASI~1\
CCS\ccs1100\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Oct 8 2021'.
The library build time was '18:03:35'.
The library package version is '9.5.0.00143'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End: Texas Instruments XDS2xx USB Debug Probe_0]
Clément