Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Hello C2000 gurus,
I would like to implement a firmware upgrade feature on a F2837x device over CAN. I am using these two well written app notes as my reference: SPRACN1, SPRABV4E. I found a MCAN example (CAN Flash Programmer) for F28003x device, which seems to be (functionally) very close to what I want to implement on the F2837x device. Found here: \\C2000Ware_4_03_00_00\driverlib\f28003x\examples\flash
Do you have a similar example for any of the DCAN devices available (even if not in final C2000Ware ready form)? If not, how big of a jump would it be to use the above MCAN example as reference for the F2837x device?
Are there any other examples I should use instead?
Thanks,
Hrishi