Part Number: TMS320F28388D
Hi
Using the controller TMS320F28388D , would like to know the connection for boot pin is correct or not .
Page 75 says GPIO72 can also be used as D12 (EMIF1_D12) for SDRAM communication.

Also Page 259 says GPIO 72 should be permanently high for USB boot.

So How can I make D12 permanently high on board if I wish to have data transfer between SDRAM and MCU.
Please help me to resolve this query.
Regards,
Sooraj