Part Number: TMS320F28032
Hello, I asked this question yesterday, however, I may have failed to complete the Form because, I did not see my question posted. Therefore, I will ask again.
When using the TI, TMS320F28032 Micro Controller, could I use the GPIO30 [ CANRXA [ I ] port [ pin 33 ] to bias a Transistor ON [ MMBT3904WT1 ] ?
Would it be better if I used the GPIO31 [ CANTXA [ O ] port [ pin 32 ] instead ?
The reason I am asking is because the Data Sheet lists CANRXA as an Input [ I ] and CANTXA as an Output [ O ]. Is the " I " and " O " labels only regarding, interfacing these ports to communication devices ?
Thank you and good day.
Robert J. Kukis
robert.kukis@rockwellautomation.com