Part Number: TMS320F28388D
Hello;
Based on the F28388D's datasheet, there are 4 ADCs in it, and each ADC has 16 SOCs, so there are total 64 SOCs. Is this correct?
So if I want to setup the ADC-A's SOC3 to acquire the analog signal on pin ADCINA5(pint# T3 of 337-ball ZWT package). Is the following C statement correct?
ADC_setupSOC(ADCA_BASE, ADC_SOC_NUMBER3, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN5, 80U);
Also can I setup the ADC-A's SOC5 to acquire the analog signal on pin ADCINA5(pint# T3 of 337-ball ZWT package)? And the C statement is as following?
ADC_setupSOC(ADCA_BASE, ADC_SOC_NUMBER5, ADC_TRIGGER_EPWM1_SOCA, ADC_CH_ADCIN5, 80U);
Thanks
Wen Li