This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: Start up code

Part Number: TMS320F280039C

Hi Team, 

Can you please check the inquiry below?

A customer tried to edit the startup files to set ram sections to zero, during debugging they noticed that the debugger ignore the code they wrote to initialize the ram, after so search they found out they have to Generate a library using the mklib in the direction C:\ti\ccs1210\ccs\tools\compiler\ti-cgt-c2000_22.6.0.LTS\lib …now the debugger can see the added code but the problem is that when they try to initialize any ram section even if it is empty the microcontroller goes an error Saying no source available for "system post cinit.  

Can you help? 

Thank you kindly.

Regards,

Marvin