This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: CAN messages receiving - which one was first - time stamp

Part Number: TMS320F280049


Hi All,

I have been using CAN on 280049 for long time, but now I am facing new challenge.

I have configured CAN message objects (mask, filters...) receiving/transmitting works well.

I reading CAN messages in main loop, in ~1ms interval. Works fine, until control system do not send many messages in the row, with no delay between.

When I am going read messages, I can see for example 6 messages received. As in each message is counter, I must know order of messages. On 28065 device, there is Message Object Time Stamp register, so I can sort out messages according time.

Is on 280049 device something like this?

I do not want to use interrupt on CAN, as my application is time critical (power converter), CAN bus shall be task with minimal priority.

Thank you

Best Regards

Martin Pietka