This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Flash the CM-core without touching other cores.

Part Number: TMS320F28388D

When I want to start a debug session in css, with only the CM-core. (Assuming the CPU1 core is already running the cm_config binary). It seems not possible to debug this core (standalone). When I watch the progress of erasing, writing the flash, it seems that CPU1 is erased when I start the debug sessions on the CM-core. I could not find any documentation about these steps. Is this right? Is it not possible to flash/debug the CM-core as standalone core, without erasing CPU1?