Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Dear TI,
I'm using F28388D control card and trying to boot basic application (freertos_ex2_c28x_led_blinky from C2000ware) from flash.
Below are the steps I'm following.
1. Import the freertos_ex2_c28x_led_blinky example from C2000ware to CCS. Set the build configuration to CPU1_FLASH.
2. Power the emulator and MCU. Switch settings on board is (S1:A position 1: ON, S1:A position 2: OFF)
3. Build the example and flash through CCS. LEDs start blinking.
4. Power cycle the board with switch settings (S1:A position 1: ON, S1:A position 2: OFF).
5. Power cycle the board with switch settings (S1:A position 1: OFF, S1:A position 2: OFF).
After both steps 4 and 5, I do not see LEDs flashing. I maybe missing something here and it could be silly mistake.
Please help in this regard on how to boot the code from the flash and to make run after power cycle.
Thanks beforehand.
Regards,
Rakshith