Part Number: DRV8301-69M-KIT
Hello There,
I am running DRV830x-HC-C2-KIT with INSTASPIN-FOC GUI
IN the GUI when we click on "Identify the motor parameter" button, then GUI is showing DRV fault status RED and Reset DRV fault is not working.
I have set the "Motor identification Parameter" as following:
- Res Est current (A) : 4.5
- Ind Est current (A) : -4.5
- Estimate Freq (Hz) : 20
- Motor Pole pair ; 21
- Motor max current(A): 45
- Motor max freq (Hz) : 1500
BLDC motor parameter :-
- Max voltage (volt) ; 12S
- Max current (Amp); 68.6
- Max RPM: 4123
- Poles :42
Kindly suggest me what could be the issue and how to resolve it?