This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28335: TMDSCNCD28335

Part Number: TMDSCNCD28335

I Try to run the DSP oscilloscope  in PSIM with f28335 the PSIM example called " Monitoring 3-phase Sine Waveform through
SCI (Serial Communication Interface)" .So, I turn SW1 off and short J9  in F28335 then generate the code but when I click on connect in DSP oscilloscope, it shows an error  "Connection to DSP can not be established" so it did not work.

Kindly, I need your help with that!