This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Linker command file location

Part Number: TMS320F28388D

Hi Experts,

Our customer has a concern, to organize his project he has decided to put the linker command files into ${PROJECT_LOC}/2838x_RAM_lnk_cpu1.cmd. So into the project properties he set this: 

With the ${PROJECT_LOC} configured as follow:

 

When he build the project it does not use his file and go back to the properties it was modified to empty:

 

He also tried to manually set the location using the `browse` button: 

But again the information isn't held. What is the issue?

It seems he don't need to do ${PROJECT_LOC}/cmd/*.cmd, but just `cmd/*.cmd`. In this case it only work if he doesn't have several .cmd files in the same location, for instance he have flash.cmd and ram.cmd, he configured the configuration to use cmd/ram.cmd, but as long as the cmd/flash.cmd is in the folder, the configuration uses-it. Why?

Please advise. Thank you.

Best regards,
Gerald