This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157-Q1: CAN communication issue

Part Number: TMS320F2800157-Q1
Other Parts Discussed in Thread: TMS320F2800157, C2000WARE

Hello,

    We are using TMS320F2800157 IC for the project, We wrote CAN code for communication( data rate of 500kbps ). We are having our developed board The CAN communication is working fine on 1 board out of 3 along with the whole software, for remaining 2 boards the conditions are like below:

1) On 1 board the CAN signal is not coming on the CAN TX pin itself (Checked with Digital Oscilloscope), Remaining all peripherals is working fine.

2) On remaining 1 board the CAN communication will start working but after some random time span the CAN communication will stop automatically (No signal on CANTx pin) but the remaining software will work continuously without any error.(it will restart CAN communication after Resetting the controller) 

The same boards are tested with the TI C2000Ware_4_01_00_00 library CAN example code & also for different bit rate of CAN the result for CAN communication is same.